Cancel
Showing results for 
Search instead for 
Did you mean: 

Technical/ Development Support

N/A

I have been in touch with two individuals over the past few days with this delayed commands issue... one said to try setting Application Display on graphic card set all nothing. They both said to check with Developers for Solid Edge...So, if there is a developer with knowledge of Graphic Cards feel free to get in touch, Please. This is a video which is slower yet.

http://screencast.com/t/exv69bmdy

This video is the Graphics Card and the description of this computer

http://screencast.com/t/DNUfAZkT

Thanks
Crousie

2 REPLIES

Re: Technical/ Development Support

Esteemed Contributor
Esteemed Contributor
Crousie, is your drawing by chance really big with lots of geometric and dimensional constraints?


Ken

Production: ST10 MP5
Testing: SE 2019

Re: Technical/ Development Support

N/A
Good Morning Ken,
Yes this drawing has all the above, (48 in. x 25 in.) The drawing is being done on synchronous part, building and modeling.