Cancel
Showing results for 
Search instead for 
Did you mean: 

Technical Requirements tool - multiple columns?

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

Hey I was just wondering if anybody uses the Technical Requirements tool in the draft environment?  I am putting a tech. spec onto a drawing and it is long enough that I need to make at least one additional column.  Otherwise it will  be "too tall" for the drawing andwon't fit.  It looks like there is no option for multiple columns unless somebody know otherwise?  The only other way is to make a second technical requirements but then it has to go on a different sheet which is a pain because I want to fit the whole thing on one sheet.  Am I SOL?

 

 

 

Cheers,

 

Chris

3 REPLIES 3

Re: Technical Requirements tool - multiple columns?

Siemens Phenom Siemens Phenom
Siemens Phenom

Master ER # 7525359 - Technical Requirements textbox to span multiple columns / multiple sheets

Re: Technical Requirements tool - multiple columns?

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

@uk_dave, thanks for that.  I have asked my VAR to add me to it.

Re: Technical Requirements tool - multiple columns?

Gears Phenom Gears Phenom
Gears Phenom

There must be many more Tech Specs enhancement requests to make it more word processor friendly.  Things like hanging indents, multi-level notes (1, 2, 2.1, 2.2, 2.3, 3, 4, etc. for example; or 1, 2, 2a, 2b, 2c, 3, 3a, 3b, etc.), and forced carriage returns within a note.

 

Those are 3 off the top of my head.


____________________________________
--Scott Wertel, P.E.