Cancel
Showing results for 
Search instead for 
Did you mean: 

Teeth disappears when importing into assemblies.

Valued Contributor
Valued Contributor

Hello ST8 SE community

 

I am trying to create an assembly of different gears that I made using the gear option in the solid edge assembly enviornment. When I try to import the part into a new enviornment, the teeth around the gear dissapperars, and I only have a circular disk. I have tried hide-all/show-all option from the right click but no luck yet. The moment I creat the gear, it is visible but when I am trying to import it to a new assembly enviornment, it dissappears. It will be really helpful if you can provide the soluction. 

 

Thank you!

Screenshot (36).png

 

 

Screenshot (37).png

 

 

 

2 REPLIES 2

Re: Teeth disappears when importing into assemblies.

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi there,

 

It has switched to a simplified view to reduce weight of the assembly.

Right click on the top level assembly in the Path Finder and select simplified/adjustable>Use Designed Parts.

 

Regards,

Jonathan

Re: Teeth disappears when importing into assemblies.

Valued Contributor
Valued Contributor
Thank you so much!!!