Cancel
Showing results for 
Search instead for 
Did you mean: 

Template Setup

Experimenter
Experimenter
Hi,
I have a question regarding the default options when you click on the down arrow next to the Hole options. The part template has the hole option defaults for the drop down set, somehow in the template but the sheet metal templates have only the defaults.
How do you choose to save the defaults in the sheet metal template? When I try to save a hole configuration in the sheet metal template, it seems to create a file called custom.xml but whoever did this before me managed to get them saved in the part template.  I am, unfortunately, still running an 'antiquated' v18!!
Thanks
1 REPLY 1

Re: Template Setup

Siemens Creator Siemens Creator
Siemens Creator

  The holes are added to the drop down list by using the “Save” button under “Saved Settings” on the hole options dialog.