Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Termination log error solid edge v20

Experimenter
Experimenter

I'm facing this error what i do??? Even i couldn't perform any task on it and 4 labs gone. Please help me as soon as possible. I'm using window 10.

3 REPLIES 3

Re: Termination log error solid edge v20

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Your issue is that you are running Solid Edge v20 on Windows 10. V20 only supported Windows XP and Windows 7. You have 2 choices. Upgrade Solid Edge to the latest or downgrade your PC to Windows 7.


Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: Termination log error solid edge v20

Experimenter
Experimenter

how to upgrade an solid edge

Re: Termination log error solid edge v20

Siemens Phenom Siemens Phenom
Siemens Phenom

@lvelyjagu please do not cross- and double post on the forum.  You are already actively engaged on this forum for your issue under the following post:

 

https://community.plm.automation.siemens.com/t5/Solid-Edge-Forum/Need-help-to-use-Silid-Edge/m-p/452...