Cancel
Showing results for 
Search instead for 
Did you mean: 

Text location

Not applicable

Hi all.
Is there a way to place text close to a certain geometry object (a point for example),
and have it stay close to it even if you move/rotate the geometry?
The relationships do not seem to work with text as they do with geometry (to align
the text with a point for example).
Or should I use another tool to achieve this goal?
Thank you
Cedric.
2 REPLIES 2

Re: Text location

Not applicable
Use a callout with leader turned off in place of a text box. First click is
to select the anchor point for the callout. 2nd click is to place the text.
The text will stay in the same relative position to the anchor point when
the geometry moves.
David
"Cedric Groyer" wrote in message
news:47be95b1$1@bbsnotes.ugs.com...
>
> Hi all.
>
> Is there a way to place text close to a certain geometry object (a point
> for example),
> and have it stay close to it even if you move/rotate the geometry?
> The relationships do not seem to work with text as they do with geometry
> (to align
> the text with a point for example).
>
> Or should I use another tool to achieve this goal?
>
> Thank you
>
> Cedric.


Re: Text location

Not applicable

Thanks David.
That seems to be a great solution!
I'll try that further later on.
Thanks again.
Regards

"David Rieschick" wrote:
>Use a callout with leader turned off in place of a text box. First click
>is
>to select the anchor point for the callout. 2nd click is to place the text.
>
>The text will stay in the same relative position to the anchor point when
>
>the geometry moves.
>
>David
>
>"Cedric Groyer" wrote in message
>news:47be95b1$1@bbsnotes.ugs.com...
>>
>> Hi all.
>>
>> Is there a way to place text close to a certain geometry object (a point

>
>> for example),
>> and have it stay close to it even if you move/rotate the geometry?
>> The relationships do not seem to work with text as they do with geometry

>
>> (to align
>> the text with a point for example).
>>
>> Or should I use another tool to achieve this goal?
>>
>> Thank you
>>
>> Cedric.

>
>