Cancel
Showing results for 
Search instead for 
Did you mean: 

The best Mice for CAD software users

Gears Phenom Gears Phenom
Gears Phenom

Hi,

I am looking to buy a mouse to operate Solid Edge.

So far I am using standard 3 key mouse, but thinking about something more accurate.

What preferences do you have ?

 

thanks for the advise.

Arek

 

15 REPLIES

Re: The best Mice for CAD software users

Honored Contributor
Honored Contributor

Very personal decision. Most like different mice because we all have different size hands.

 

I settled into Logitech G700. About 7 years ago I decided I liked that mouse and purchased four of them. One for work and two for home and one in the car as back up wherever I am.

 

The main feature I like about it is the wide and flap-topped wheel that can also be used for side to side input.

Re: The best Mice for CAD software users

Legend
Legend

A 3D mouse is nice to have, and there are some cheaper versions out there, but I use this brand at work and at home.

 

http://www.3dconnexion.com/

Re: The best Mice for CAD software users

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@arekkul,

 

We've used the Logitech MX1000 and now the newer MX800 [combo] units for many years, as have good precision, comfortable size & shape, cordless, and have numerous programable buttons......I also have a 3D Connexion Space Pilot for while I'm docked at the office.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: The best Mice for CAD software users

Creator
Creator

The 3Dconnection Cadmouse is a very nice mouse and I have used the above mentioned creaters and the Cadmouse really works well even with big hands

Re: The best Mice for CAD software users

Gears Phenom Gears Phenom
Gears Phenom

Hi @bhaskin,

 

Can you tell us a bit more about the Cad Mouse from 3DConnection ? I am thinking about this particular mouse, but it is quite expensive compare to the rest.

 

Thank you,

 

Arek

 

Re: The best Mice for CAD software users

Valued Contributor
Valued Contributor

I've been using a Logitech Cordless Optical Trackman for the last ten years. It was an arm saver from the standard type mice. Only downside is they have stopped making it, so I purchased a few to last me and now down to last one.  I have no idea what I will chose to use when it needs replacing (when the left mouse button packs up from the endless mouse clicks we have to do)...

Re: The best Mice for CAD software users

Phenom
Phenom

I have a Cad Mouse from 3DConnection, in the closet...

I suffer RSI, and this mouse doesn't help.

Therefor I use a wacom tablet. At the office a very old bamboo fun and at home a intuos 3.

I also use a classic mouse with my left hand and a spacepilot pro to navigate.

A perfect setting for me. There is more for inpunt than a mouse. A 3D mouse is for me a must.

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user

Re: The best Mice for CAD software users

Legend
Legend

And, for a regular mouse, I have used the Logitech trackball for the past 15+ years. I can't stand having to pick up the mouse, over and over, so I like just rolling my thumb to move the pointer.

 

https://www.logitech.com/en-us/product/wireless-trackball-m570

Re: The best Mice for CAD software users

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

I'm using a Logitech cordless mouse.  For me, a basic 3 button/wheel mouse works fine.  More important to me is my 3D Connextion Space Mouse Pro.  Being able to manipulate views with it is second nature.

 

Unfortunately, I can't say the same about the 3D Connexion CAD mouse.  I used one while taking the certification test at SEU2015 and by the time I was done, my hand was killing me. 

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1