Cancel
Showing results for 
Search instead for 
Did you mean: 

The magic of Synchronous

Legend
Legend

Picture a customer that demands a Dual bracket for (several) vibration switches...  a bracket that is done in Solid Edge Sheetmetal.. 

 

Watch our standard bracket transforming from single mount to dual mount within approx. 30 seconds.... and then image how much time that would have taken in ordered mode.. or in SW or Inventor..

 

This made me smiling a few minutes ago and I would like to share this.

 

Merry Christmas and a Happy and Healthy year to all of you.

 

Jan Bos

Solid Edge user since V3.5 and beta tester for ST10

Emmen, The Netherlands

 

 

(view in My Videos)

10 REPLIES 10

Betreff: The magic of Synchonous

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Jan_Bos

 

 

 

let me say "Thank You" for the same smile You brought onto my lips with this video
and with Your statement for Sync

 

I hope that we can bring more of this Sync "lights" to screen in the "New Year 2017!"

 

Also a

"Merry and peaceful Christmas and Happy New Year 2017!"

to all Edgers and to this community

 

Smiley Happy

 

regards
Wolfgang

Re: The magic of Synchonous

Gears Phenom Gears Phenom
Gears Phenom

@Jan_Bos perfect! This is what (we) I like in synch and competitors hate! Smiley Wink

 

Merry Xmas & Happy New Year!

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: The magic of Synchonous

Honored Contributor
Honored Contributor

I would love to use Sync, but there are things I have yet to figure out how to do in sync so I stay away from it.

 

Attached is a very simple example. How would you create this from scratch in sync?

The goal is a single angled cut (in the flat) including how it goes around the corners. In that way, the part is easy to make with a punch. The term I use for it is "crisp" flat patterns.

 

The attached part is not practicaly useful. But it does get right to one of my general problems.

 

 

 

 

Re: The magic of Synchonous

Gears Phenom Gears Phenom
Gears Phenom

Here is what I would do. Did have to switch over to ordered to do the unbend.

 

Didn't fully constrain anything, was working quick.

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Re: The magic of Synchonous

Gears Phenom Gears Phenom
Gears Phenom

then I just made one that was more like what you did from the start.

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Re: The magic of Synchonous

Gears Phenom Gears Phenom
Gears Phenom

I just realized there is no way you could know what I did to make this in synch. Drew the flat profile. Made it into a tab. Drew my lines to bend on the tab. Then used bend and selected the line, chose the side to move, hit enter, rinse and repeat for the next bend.

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"
Highlighted

Re: The magic of Synchonous

Honored Contributor
Honored Contributor

If I need to use mixed mode to do anything in sheet metal, using a mixture of Sync and Ordered sounds much more complicated than sticking to just ordered. 

 

My question was how to create the simple part using nothing by sync, apperantly the answer is "you cant". I consider that  a VERY simple part. Once a cut is needed that goes across a bend, sync cany be used by it's self to create the feature. I have half a dozzen other specifics w/ sheet metal design that can't be done w/ sync. almost all of it relates to the flat pattern size and shape. There are no flat pattern controls w/ Sync. 

Re: The magic of Synchonous

Gears Phenom Gears Phenom
Gears Phenom

@12GAGEI made the second model I attached entirely in synchronous. I don't like how i did it however. I don't like drawing the part flat and then bending it. But it was done entirely in synch.

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Re: The magic of Synchonous

Gears Phenom Gears Phenom
Gears Phenom

@12GAGE wrote:

If I need to use mixed mode to do anything in sheet metal, using a mixture of Sync and Ordered sounds much more complicated than sticking to just ordered. 

 

My question was how to create the simple part using nothing by sync, apperantly the answer is "you cant". I consider that  a VERY simple part. Once a cut is needed that goes across a bend, sync cany be used by it's self to create the feature. I have half a dozzen other specifics w/ sheet metal design that can't be done w/ sync. almost all of it relates to the flat pattern size and shape. There are no flat pattern controls w/ Sync. 


The main reason I don't use sync is that it cannot do lofted flanges. If it can't do lofted flanges what's the point in learning it at this stage because I do lofted flanges all the time. Every job almost has at least one. Doesn't make much sense doing everything else in sync, which I don't know very well, when ordered does it in a more controlled fashion and does it all completely.

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"