Cancel
Showing results for 
Search instead for 
Did you mean: 

The same parts repeated in pathfinder

Valued Contributor
Valued Contributor

hi~users..

There are repeated parts in the assembly, such as the title.
This is not to represent each one ...
I want the same parts to be represented in one.
I just want to be able to check the quantity used for the count.

Is there any option in ST9 version?

ss11.png

6 REPLIES

Re: The same parts repeated in pathfinder

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi @Hclee

 

You can right-click on the parts and pick 'Group' from the context menu.

Then rename the group to same as the parts.

 

Counting is not possible directly from the group though and you still have to use the Reports command on the Tools tab.

 

Tushar

 

Re: The same parts repeated in pathfinder

Valued Contributor
Valued Contributor

Thanks Tushar
If there is only one list of parts, the length of the passfinder is shortened
It will be more convenient.
I guess there's only one way ...

Re: The same parts repeated in pathfinder

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi @Hclee

 

I did not understand your last message.

Nor it is clear if you found grouping option in PathFinder useful.

 

Tushar

Re: The same parts repeated in pathfinder

Siemens Phenom Siemens Phenom
Siemens Phenom

No, it is not possible. Each occurrence of a part can have completely different occurrence properties, positions, relationships, etc. There is no way to maintain that uniqueness if you simply have a single entry in the Pathfinder that represents all occurrences of that part. If your goal is to reduce what you see in Pathfinder, Groups are probably your best option as Tushar suggested.

 

Greg

Re: The same parts repeated in pathfinder

Gears Phenom Gears Phenom
Gears Phenom

Hello,

 

Would it be possible to pattern or use the "duplicate" command to pattern the parts in the assembly?  If so, you would have on part in the tree.

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1

Re: The same parts repeated in pathfinder

Gears Phenom Gears Phenom
Gears Phenom

If you want to check quantities in the assembly on the fly, you can pick on of the parts and then go up to the "select" pane and use the "select all identical parts"  the count will show at the bottom of the screen.

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1