Cancel
Showing results for 
Search instead for 
Did you mean: 

Thin Wall in Vehicles

Experimenter
Experimenter

Hello,

 

I am trying to use the thin wall feature on the vehicle attached; however, I keep getting different errors such as:

"The face geometry has resulted in an unsupported condition. Make sure the faces properly intersect the part."

"Thinwall failed. Adjacent faces do not intersect when offset."

The bottom surface of the car has different angles, for this reason I have tried selecting all the faces or just one but it still doesn't work.

Could someone please help me?

 

Thank you!

FS

 

1 REPLY 1

Re: Thin Wall in Vehicles

Gears Phenom Gears Phenom
Gears Phenom

can you share your model so that we can "play" with it.

 

 

 

 


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7