03-14-2014 10:36 AM
Is there a way I can show the dashed thread indicator in an Isometric view as shown in the PDF. The PDF drawing was done is SolidWorks. Looking for Solid Edge's version of doing this.
Please help.
03-14-2014 01:21 PM
that thread was physically modeled.
If you model the feature then yes you can show it just liek that...
but most eveyone only represents threads... to save PC resources.
03-14-2014 01:48 PM - edited 03-14-2014 01:59 PM
I see what you are referring to, I don't mean the actual modeled thread. I mean the dashed elipses at the two holes on the body. Those are pipe ports for air lines. I need those dashed lines to represent the cosmetic thread without changing the view shading
See attached edited PDF
03-19-2014 08:14 AM
Hello,
Can you project a dashed circle onto the countersunk surfaces in the model and then show the sketches in the draft?
Kyle