Thread indicator in Isometric

Is there a way I can show the dashed thread indicator in an Isometric view as shown in the PDF.  The PDF drawing was done is SolidWorks.  Looking for Solid Edge's version of doing this.

 

Please help.

Owner: Scott Lester Drafting & Design
Designer: Rotork Instuments
3 REPLIES

Re: Thread indicator in Isometric

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

that thread was physically modeled.  

 

If you model the feature then yes you can show it just liek that...

 

but most eveyone only represents threads... to save PC resources.

Matt Johnson
Application Engineer
Ally PLM Solutions
matt.johnson@allyplm.com
http://allyplm.com/

Re: Thread indicator in Isometric

I see what you are referring to, I don't mean the actual modeled thread. I mean the dashed elipses at the two holes on the body.  Those are pipe ports for air lines.  I need those dashed lines to represent the cosmetic thread without changing the view shading

 

See attached edited PDF

Owner: Scott Lester Drafting & Design
Designer: Rotork Instuments

Re: Thread indicator in Isometric

kjoiner 1st Gear
1st Gear

Hello,

 

Can you project a dashed circle onto the countersunk surfaces in the model and then show the sketches in the draft?

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1