Cancel
Showing results for 
Search instead for 
Did you mean: 

Thread

Experimenter
Experimenter

Hello,

 

I use Solid edge ST9.

And for some reason if I select thread it is green instead of showing real thread.

Knipsel.JPGIt should show normal M8 thread

Is there anyway I can let it show "normal" thread like this?

Knipsel.JPGLike this

 

Are there settings I have to adjust or something?

3 REPLIES

Re: Thread

Phenom
Phenom

Go to the View Tab and select View Overrides. Make sure Textures is checked.

Bob Henry
REH Technical Consulting
Canonsburg, PA 15317

Re: Thread

Experimenter
Experimenter

Thank you!

Re: Thread

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Henky  Just making sure you know it's not a "real" thread. It's just a texture, a picture if you will.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200