Cancel
Showing results for 
Search instead for 
Did you mean: 

Threaded Hole Color

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

When we create a threaded hole feature the face color is cyan. That's fine and good but what controls that color?

 

ThdHoleColor.JPG

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200
2 REPLIES

Re: Threaded Hole Color

Gears Phenom Gears Phenom
Gears Phenom

There is a Face Style "Thread" that controls that.

 

1-10-2018 9-49-19 AM.png


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Threaded Hole Color

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

OK. Thanks for that. You have to hit modify to see it. Wonder why the color for thread doesn't show what it is in the styles window? I click on thread and it's grey.

Or was grey. Discovered that a texture setting was overriding the underlying color.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200