Cancel
Showing results for 
Search instead for 
Did you mean: 

Threads and exporting as STL

Experimenter
Experimenter

Hi

 

I'm currently using solid edge to create .STL files fo rmy 3d printer. The only issue i am having at the moment is that threads do not appear on the STL file.

Is anyone else having trouble with this?


Thanks in advance

 

4 REPLIES

Re: Threads and exporting as STL

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Threads created in SE using the thread command are only metadata and a view style mapping.  No physical threads are created in the 3D.

 

If you need to have the threads in your printed model you will need to create them physically by way of helical command.

 

HTH

Matt Johnson
Application Engineer
Ally PLM Solutions
matt.johnson@allyplm.com
http://allyplm.com/

Re: Threads and exporting as STL

Experimenter
Experimenter

thanks for the reply, is there a tutorial on how to do this?

Re: Threads and exporting as STL

Community Manager Community Manager
Community Manager

It is not very complicated. Just search the help for Helical and I am sure you will come up with the help on how to do a helical cutout.

Dan Staples
Director, Solid Edge Product Development

Re: Threads and exporting as STL

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Youtube is your friend. Smiley Wink

 

You need helical protrution or cutout.

 

Look at this video from 8:30.

 

 

BR,

Imi

Imics
http://solidedgest.wordpress.com/