Cancel
Showing results for 
Search instead for 
Did you mean: 

Threads in a draft file

Creator
Creator

I'm using ST5 when I create threads in a .par file, shouldn't they appear in the .dft file as well or do I need to add them to the .dft file.  Any help is greatly appreciated.  Thanks.

2 REPLIES

Re: Threads in a draft file

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Assuming you are using the Hole command or the Thread command and not actually creating physical threads.  They should show up in drawing views using the typical annotation for the standard you are using (ANSI, ISO, BSI, etc...).

2016-01-14_10-38-32.png



Ken

Production: ST10 MP7
Testing: SE 2019
http://Grundey.blogspot.com

Re: Threads in a draft file

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @TRC,

 

Yes they should.....if they are un-shaded, then only in orthographic views....and shaded if needed to be visible in alteranate views.

 

2016-01-15.png

 

2016-01-15 (1).png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x2 seats]
Windows 10 - Quadro P2000