Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Thumbnail problem!

Valued Contributor
Valued Contributor

Why do some files show the part in the thumbnail, while other dont? For eg. here part 3 only has a previsualization.

 

Screenshot (19).png

 

 

2 REPLIES 2

Re: Thumbnail problem!

Experimenter
Experimenter

What version of Solid Edge and Windows are you using?

 

Re: Thumbnail problem!

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @AmanRa,

 

I remember having this issue quite some time ago, actually we still discover files that are like this.....so can only assume you have older files on your system.

The only way I know of, is to do an "Open/Save" on them.

 

I believe it was a Windows UAC [I think late ST7 ~ early ST8 era] issue, that was fixed in a Maintenance Pack.....not sure which one.

 

Further.....do I see "Bootcamp" on your directories? So that infers you're probably running on a Mac right??

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000