Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Tilted dimension

Experimenter
Experimenter
Is it possible to tilt dimension something like on this picture? Thanks.
https://drive.google.com/file/d/0Bwss19kUiSLuNnFSamRYMnFxaFk/view?usp=drivesdk
2 REPLIES

Betreff: Tilted dimension

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Andrija

 

 

 

this is an easy task.

 

Just go into the properties of that dimension and change the angle value for it:

 

20171031_2310.PNG

regards
Wolfgang

Re: Tilted dimension

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Yes.

  1. Place a dimension
  2. Right mouse click on it and select Properties
  3. In the Dimension Properties dialog select the Lines and Coordinate tab
  4. In the Projection Line section change the Angle field to whatever you want (45°)
  5. OK


Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com