Cancel
Showing results for 
Search instead for 
Did you mean: 

Title Block Sheet Metal Auto Populate

Creator
Creator

Hi,

 

I am using the same title block for standard parts and sheet metal parts.

In the tilte block I have the bend radius and K-factor code shown.

%{Bend Radius|R1}
%{Neutral Factor|R1}

This is fine when I have a sheet metal part. When I have a standard part these codes show 'Error: No reference'.

 

Can I have 'N/A' or '-' show in its place when a sheet metal part is not used?

5 REPLIES 5

Re: Title Block Sheet Metal Auto Populate

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

You can do it. Open a draft & SE app button -> Settings -> Options -> General -> "Property text editor" -> Show my error: N/A. Apply all changes.

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Title Block Sheet Metal Auto Populate

Creator
Creator

Thanks for that solution.

It took me a little while to find the Property Text editor as it was called property text error lol

Re: Title Block Sheet Metal Auto Populate

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Imics, for some reason those settings are greyed and not changeable on my system. Do you know if it has to do with Insight?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Title Block Sheet Metal Auto Populate

Siemens Phenom Siemens Phenom
Siemens Phenom

@bshand check the setting in your options.xml.

Re: Title Block Sheet Metal Auto Populate

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

That's the first thing I did but apparently suffered momentary blindness. Now I see it. Thanks. I wish seadmin had a find function.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200