Cancel
Showing results for 
Search instead for 
Did you mean: 

To Bend a Strap

Creator
Creator
Hi, I recently designed and 3D printed a flat rubber foot strap. However I would like to Bend it when shown in the assembly on top of the boot. Is there any commands available to do this or way to flex the part?
Thanks
1 REPLY 1

Re: To Bend a Strap

Gears Phenom Gears Phenom
Gears Phenom

Possibly...  depends on how much you need to bend it and the tangencies between the sections.

 

You could model in a sweep and adjust the part from the assy. 

 

Can you share some basic dims and screen shot or image?

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7