Cancel
Showing results for 
Search instead for 
Did you mean: 

To increase the draft angle for the complex profile using synchronous Technology

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi 

  I am having a model with complex profile(File size around 14 MB). My system configuration is i5 Processor 8GB RAM and 4GB grahix card. This profile is having -1.5 degree(negative) draft angle at its Surface and I would like to make it as positive draft angle (ie +1.5 degree). Even though i am having this configuration I couldn't able to get solution. Please tell appropriate solution

2 REPLIES 2

Re: To increase the draft angle for the complex profile using synchronous Technology

Gears Phenom Gears Phenom
Gears Phenom

I would suggest removing the rounds 1st.  Then attemp the draft edit...


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: To increase the draft angle for the complex profile using synchronous Technology

Gears Phenom Gears Phenom
Gears Phenom
Hi,

Really? Positive draft means you will have an undercutted area... Of course it depends on opening direction.

BR,
Imics
http://solidedgest.wordpress.com/