Cancel
Showing results for 
Search instead for 
Did you mean: 

Tool tip for PathFinder

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

The tool tip that appears when hovering over an item in the PathFinder lingers for about 8-10 seconds and cannot be dismissed by clicking or double clicking on it. Zoom or refresing using F5 also does not help. Pressing the Escape key also is of no use.

Is there a way to dismiss it or some setting for the duration for which it appears. I looked through the Options dialog but did not find any.

TipLingers.png

3 REPLIES

Re: Tool tip for PathFinder

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
My guess it is graphics card related. Check your driver or switch SE options to backing store.


Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com

Re: Tool tip for PathFinder

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor
Thanks Ken for the clue. I tried it out.
I have an ATI Radeon HD 5450 (driver ver. 8.821.0.0) but not sure if it makes the cut for minimum requirements for ST6.

Re: Tool tip for PathFinder

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor
Meanwhile, I figured out that moving the mouse over another PathFinder item like a Reference Plane and further quickly moving out the mouse into an empty space in the graphics area dismisses the tooltip balloon in question.