Cancel
Showing results for 
Search instead for 
Did you mean: 

Toolbar, when editing a part in sync

Genius
Genius

During editing a part, how do I get the toolbar visible static.

Toolbar.png

 

Today,I have to keystroke Advance to get the toolbar.

 

Toolbar_2.png

 

Solid Edge 2019
4 REPLIES 4

Re: Toolbar, when editing a part in sync

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I don't believe you can.  When the Design Intent UI was introduced, that eliminated much of the dependency on the Advanced Design Intent (Live Rules) panel and thus it is not shown by default.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Betreff: Toolbar, when editing a part in sync

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Geir-Petter

 

 

I also think that it is as mentioned by @KennyG

 

The following question will be: "Is the toolbar necessary and/or the better user inetrface than the Design Tool window?"

 

Opinions will be differ but at the moment it seems that we can not change anyting so far

 

regards
Wolfgang

Betreff: Toolbar, when editing a part in sync

Genius
Genius

I think I got the solution . During editing, I am typing "V". 

 

Solid Edge 2019

Betreff: Toolbar, when editing a part in sync

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Yes, tapping V is the shortest and quickest way to put away or bring back the full (advanced) DI panel.

Also you can selectively toggle each one using SPAC or SCAP as shown in the last image on this page.