Cancel
Showing results for 
Search instead for 
Did you mean: 

Top Level Assy Warnings for Parts with Failed Features

Valued Contributor
Valued Contributor

Is there a setting in SE ST8 to show warnings in top level assemblies of failed features of parts within it?  If so, how do I turn it on?  If not, how do I push for the implementation of it?

 

Let's say I have a part "A" that I'm modifying the O.D. on.  I make the modification.  Now my die part (driven by part 'A') has a failed feature as the collinear constraint between the part "A" O.D. and the I.D. of my die part is lost.  Creo and I think Solidworks will show the parts in red in the assembly to warn the user of failed features.  SE shows nothing.  It seems it's up to the user to examine each part in the assembly.

 

Thanks,

 

Matt

13 REPLIES 13

Re: Top Level Assy Warnings for Parts with Failed Features

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

No setting that I know of for failed features. Just the Error assistant for failed assembly relationships.

You could contact your reseller and have them file an ER(Enhancement request).

How about a macro that would scan the active assembly for component issues?

LMGi
www.TLMGi.com

Re: Top Level Assy Warnings for Parts with Failed Features

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

The tree does show you something wrong. Yes it doesn't show up red or in bold but, it is there. I also make sure everything related by looking at the tree.

Re: Top Level Assy Warnings for Parts with Failed Features

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@TDB,

That's not the tree though. That's the mates display for that specific part. You would have to click on every part to see it AND that only reveals problem mates not failed features.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Top Level Assy Warnings for Parts with Failed Features

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

That would be a good addition to the assembly tree......it must be some what available in the depths of code.

Something akin to the grey box error displayed in draft. [although part level errors can be discovered by browsing the "Component Tracker"....does get a little tedious spotting those errors on large assemblies]

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Top Level Assy Warnings for Parts with Failed Features

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@SeanCresswell, I haven't used component tracker much. Does it reveal failed features in the parts in the tree?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Top Level Assy Warnings for Parts with Failed Features

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Until the functionallity part of Solid Edge, here is a macro to identify failed features in the context of an assembly.

You can download it here.

https://fffse.codeplex.com/

I would ask that you use some caution in testing, like saving your assembly first.

The macro does not alter any files but it does activate components in order to access geometry.

Regards,

Jason T.

 

LMGi
www.TLMGi.com

Re: Top Level Assy Warnings for Parts with Failed Features

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@bshand wrote:

@SeanCresswell, I haven't used component tracker much. Does it reveal failed features in the parts in the tree?


 

Oh darn it, I just ran a small test case......I was wrong, it seems to only track file structure / links.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Top Level Assy Warnings for Parts with Failed Features

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@JasonTitcomb  Only parts defined in context? What about just parts with failed features?

@SeanCresswell  Oh, well, thanks for trying.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Top Level Assy Warnings for Parts with Failed Features

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I think @MattSs use case make sense.

If you have an assembly with inter-part links, it's possible to break other parts while modifying the assembly.

If you have a part open in the Part environment then you would use the Error Assistant.

LMGi
www.TLMGi.com