Cancel
Showing results for 
Search instead for 
Did you mean: 

Top Level assemblies

Experimenter
Experimenter

Hi All, 

 

Just installed ST8 and was very exctited to try the Top Level assembly feature, question is how do you set which assembly is a top level assembly? At the moment all assemblies are top level.

 

Thanks, 

 

Mike

3 REPLIES

Re: Top Level assemblies

Experimenter
Experimenter

So I just had a support call to my VAR about this... turns out it's an intelligent system, not sure the criteria that it selects the top level assemblies from as I have assemblies that are buried 5 deep... oh well.

 

Smiley Sad

Re: Top Level assemblies

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Are you using a data management system?

 

From update training.

  • This is only available for unmanaged files on disk.
  • Provides a very fast way to locate the top level
    assembly in a folder that has hundreds of assembly files.
  • To qualify to be a top level means the assembly
    is not apart of another assembly within that folder.
LMGi
www.TLMGi.com

Re: Top Level assemblies

Experimenter
Experimenter

Nope.

 

That's the odd thing, the connector is 4 levels down.