Showing results for 
Search instead for 
Did you mean: 

Topo Tools - App for Developers


Hi Folks:


Sharing a small utility that I developed for personal use in geometry handling - TopoTools.

This is meant for developers and not for a end-user or designer. Posting it out here for those Edgers who are also into development using Solid Edge - especially geometry and topology.



If you are not a developer and like to play around with the utility, open a part file and take the second tab called 'Highlight'. Pick an edge or face id from the list and click the corresponding highlight button. You will see the edge/face for that ID highlighted - very useful when programming especially at low level like feature edges and face manipulation.


If you forget to remove the highlight, simply run the program again and click 'Clear Highlite'.


More information in this post in the developers section.