Trace curve in Solid Edge ST6

Experimenter
Experimenter

Hello!

 

I want to know if Solid Edge ST6 has the tool "Trace curve," like Pro/ENGINEER has, beacuse I have to send a project to a teacher of mine and he told me to use this feature. The mechanism I created is the Artobolevsk's mechanism to trace the Diocle's curve (as you can see here, if you have Wolfram CDF Player plugin installed in your computer) and I have to demonstrate the curve while the system is running. I created the whole project using Solid Edge ST6 due to its simple interface.

 

If, for some reason, SE ST6 doesn't have this feature, I was thinking about changing the files format, in order to open them with ProE. Do you have any objection to this idea? Do you think it will work?

 

Thank you for any help you can provide,
Leonardo Monteiro de Carvalho

9 REPLIES

Re: Trace curve in Solid Edge ST6

Esteemed Contributor
Esteemed Contributor

SE does not have this feature.  Best you can do is plot points manually through a range of motion and then run a Keypoint Curve through them.


Thanks,
Ken

Production: ST9 MP10
Testing: ST10 MP3

Re: Trace curve in Solid Edge ST6

Phenom
Phenom

Hi,

 

Yes, Ken is right, that SE has no got such feature like tc. But SE has a very good integration with Dynamic Designer Motion from DST. SE contains tha Basic package of the DDM, but you cannot do tc from it, so you need larger package Motion and Motion Pro what can do it.

 

If you are a student then you can download student version from DDM, I think! The guys at DST are very helpful (Scott Ziemba and Jeff Arrigotti) so I suggest to contact with them! Smiley Wink

 

Here is a video, about how works it:

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Trace curve in Solid Edge ST6

Experimenter
Experimenter

Thank you guys, you helped me a lot, both you lmics and Ken!

 

Unfortunately, the teacher to whom I had to send the project doesn't have DDM installed in his PC and he did't like the idea of plotting points manually, so I had to make do with another CAD program.

Re: Trace curve in Solid Edge ST6

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I know this is an old topic.

But I recently made a small macro to create a trace path as an experiment.

Would something like this work?

LMGi
www.TLMGi.com

Re: Trace curve in Solid Edge ST6

Jason,

 

Are you willing to share your source code for this project?

 

Re: Trace curve in Solid Edge ST6

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

http://pathtracerforse.codeplex.com/

There is a ClickOnce installer also if anyone just wants to try it.

LMGi
www.TLMGi.com

Re: Trace curve in Solid Edge ST6

Jason,

 

Thank you much for sharing this tool with the community!

 

Are you able to share the source code?

 

I'm interested in learing more and this is a great example...

 

wiht or without the source code, we greatly appreciate you sharing this!

Re: Trace curve in Solid Edge ST6

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

The source is there.

Just dig in under the source code tab.

LMGi
www.TLMGi.com

Re: Trace curve in Solid Edge ST6

awesome.  thank you SO much!!!