Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Transfer option in assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @chiosa_ciprian

 

 

so, that means tha t no further issues occured since You plugged off all cables?

 

regards
Wolfgang

Re: Transfer option in assembly

Yeap, except the needy ones.... keyboard, mouse, spaceball.

Ciprian Chiosa
Solid Edge ST8 + TC10.1 - Win 7 x64
SIPA Enginnering Romania

Re: Transfer option in assembly

Phenom
Phenom
I just fought that last night for a couple hours. I even did a complete uninstall and reinstall. My "assign terminal" dialog wasn't showing up. I was using multiple monitors but set the Surface Book screen "off" and used the 24" monitor as "Second Screen Only". I had to adjust the screen setup and low and behold the dialog was on the Surface Book Screen- which was turned off by the OS! Sure wish SE would handle the dialog boxes better.

Re: Transfer option in assembly

Sometimes it happens that some windows are "hidden" under the Path Finder. Just select it, move it a little bit, and you may see the desired window.

Ciprian Chiosa
Solid Edge ST8 + TC10.1 - Win 7 x64
SIPA Enginnering Romania