Cancel
Showing results for 
Search instead for 
Did you mean: 

Transfer part to assembly and keep same place in tree and is not grounded in new assembly

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

Hello,

 

I frequently transfer sheet metal parts to new subassemblies when I add PEM hardware.  When I do this two undesireable things happen:

 

1.  The new assembly gets moved to the bottom of the tree and I have to drag it back up to where it was.

2.  In the new assembly, no parts are grounded.  If I move a single sheet metal piece to a new assebmly, I have to manually ground it before placing any PEM hardware.  If I don't the first piece flips all over the place.

 

I would like SE to keep the new assembly where the first part was located and automatically ground the first part in the new asembly.

 

Kyle

 

 

Kyle Joiner
IPA LLC
ST10 MP1
3 REPLIES 3

Re: Transfer part to assembly and keep same place in tree and is not grounded in new assembly

Pioneer
Pioneer

Does this not work?Capture.PNG

Re: Transfer part to assembly and keep same place in tree and is not grounded in new assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

"I would like SE to keep the new assembly where the first part was located"

 

You mean in the pathfinder, right, @kjoiner?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Transfer part to assembly and keep same place in tree and is not grounded in new assembly

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

Bruce,

 

Yes, I would like to keep the new subassembly at the same location in the pathfinder.

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1