08-02-2013 08:35 AM
This image shows a transparent part to the left, and a part gray to the left. Why is the left part transparent? For the advice you all gave on Add a Body and all other advice which worked perfectly. Thank You!!!
Thttp://screencast.com/t/DyNxL7WRq
Thank You
Solved! Go to Solution.
08-02-2013 09:00 AM
08-02-2013 09:04 AM
08-02-2013 09:23 AM
08-02-2013 09:24 AM
02-12-2018 04:28 PM
That link is dead.
I'm guessing the answer is similar to the NOTE at the end of:
However, even if I Activate the Solid Body, the top and bottom faces of my part still show as transparent (I can select these transparent faces).
I've tried the part painter, all the different Select types, but still nothing??
[I'm working on a part that was made from a STEP assembly file]
03-23-2018 10:01 AM
Hi Matt.
Can you please show these options in a format I can open?
03-23-2018 11:01 AM
The inactive solid body face style opacity is set by the adjustable setting accessed in Solid Edge options→View tab. If the option dim surrounding assemblies when in place activated is off, then the inactive body is shown in full opacity. If the option is on, then the inactive body is shown dimmed by percentage controlled by the slider.
03-23-2018 11:20 AM
Hi Tushar.
Thanks for this information. It works good.
One question.
If I now add it to Teamcenter, will it create 1 part or many parts (Solid Body 1-60 & Part Copy 1-70)?
That's an extra 140 parts
03-23-2018 11:25 AM
A multi-body part is one part. One file.