Cancel
Showing results for 
Search instead for 
Did you mean: 

Transparency of Imported Images

Not applicable

Hi
I have scanned an image and imported it into a drawing. The Help file says:

"When editing the properties of an inserted image or picture, the only options on
the General tab that can be changed are Transparent Color and Image Opacity."
I have found transparent color but I can't find the setting for opacity.
I am using V20.
Where is this setting likely to be?
Many thanks
Geoff
2 REPLIES 2

Re: Transparency of Imported Images

Not applicable
Geoff,
Opacity is a property of an image when it is inserted into a 3D Solid Edge
Model. Both Solid Edge and Solid Edge 2D Drafting share some resources and
help topics. If you see something in Help that you cannot find, it most
likely applies to 3d.
If there is something in help that you cannot find, please don't hesitate to
ask.
Regards,
Rick B.

Re: Transparency of Imported Images

Not applicable

Rick
Thanks for the reply. I suspected that was the case. Pity.
Cheers
Geoff

"Rick B." wrote:
>Geoff,
>Opacity is a property of an image when it is inserted into a 3D Solid Edge
>
>Model. Both Solid Edge and Solid Edge 2D Drafting share some resources and
>
>help topics. If you see something in Help that you cannot find, it most
>likely applies to 3d.
>
>If there is something in help that you cannot find, please don't hesitate
>to
>ask.
>
>Regards,
>Rick B.
>
>