Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Trim a Frame component

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

Hi,

 

Can I trim/subtract a frame component in assembly?

 

Is there a way to do it?

10 REPLIES 10

Re: Trim a Frame component

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @Arisy

 

Sure can.....the tools are on the "Features" tab, for assembly features.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Trim a Frame component

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

Hi,

 

Thanks for the reply.

 

What Feature need to use? I try to use Subtract command on frame but it not work.

Re: Trim a Frame component

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

No, you can't use the boolean tools, such as "Subtract" on regular frame entities, but you can make cutouts, etc....you'd need to right click on the frame Save As Translated, to publish to full model level component(s) if that was specifically what you needed.

 

ST8_ASM_Frame_Coutouts [Img-01].png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Trim a Frame component

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

Thanks for the explanation.

 

Actually Save as Translated is what for?

 

I attach the Picture...I want to cut the frame base on the circle on TOP. It will be easier if I can use Subtract.

Re: Trim a Frame component

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Arisy, why not just use a side or front plane, and sketch a cut based on the table top underside? [make sure "Peers" is active, if using "Project To Sketch"]

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Trim a Frame component

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

Yes...you are correct.

 

Maybe I just hoping that Solid Edge able to trim/subtract the frame components 

Spoiler
Smiley Very Happy

Re: Trim a Frame component

Pioneer
Pioneer

hi @Arisy,

 

        You can try the Exten/trim command in the frames not sure if it will solve your purpose.

 

        its inside the edit end conditions.

 

 

 

Thanks ,

 

Balaji

Re: Trim a Frame component

Honored Contributor
Honored Contributor

if the legs were made as a typical part/sweep, then you should have a solid you can use to subtract.

Re: Trim a Frame component

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

Hey @balaji1991 this is also another option I can do. Thanks