Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Trim a line2D in a sketch via visual basic

Experimenter
Experimenter

Hello,

 

I try to trim a line2d in a sketch of a part with Visual Basic with the function :

Sub Trim(x As Double, y As Double, CutObj1 As Object, Optional CutObj2 As Object = Nothing)

but the trim operation is not done on the good direction.

 

Could someones explain me what are really the X and Y parameters?

 

Thank you.

1 REPLY 1

Re: Trim a line2D in a sketch via visual basic

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Hi JMD53, you should ask this in the developer community.
Quck answer: there is a good explanation in the SESDK.chm with example code.
regards JB
regards

JB
SE 2020, VS2017