Cancel
Showing results for 
Search instead for 
Did you mean: 

Trouble Installing Student version Solid Designer ST6 on Windows 7 64bit

Experimenter
Experimenter

I do not see a 64 bit install option.  My machine has 2444 GB of free disk space and 4 GB of RAM.

 

The error I get is "The wizard was interrupted before Solid Edge ST6 could be completely installed."  The message appears immediately after pressing the Install > button at the bottom of the setup page.  I am running the installation file as administrator and also tried running in legacy compatibility modes.  The same error appears regardless.  I also followed the microsoft instructions to add full DCOM permissions to my user as suggested by Microsoft support on this issue.  No difference is observed.

2 REPLIES 2

Re: Trouble Installing Student version Solid Designer ST6 on Windows 7 64bit

Community Manager Community Manager
Community Manager

Hmmm. maybe your virus checker is blocking it or something? Worth a try...

Dan Staples
Director, Solid Edge Product Development

Re: Trouble Installing Student version Solid Designer ST6 on Windows 7 64bit

Experimenter
Experimenter
Thanks for the suggestion.  I stopped the checker and had the same problem.
 
I just noticed I wrote "Solid Designer" instead of "Solid Edge".  Aye Carumba!