Cancel
Showing results for 
Search instead for 
Did you mean: 

Trouble with defining the load-bearing face for a 3D contact constraint in DDM-SE

Experimenter
Experimenter

Hi,

 

I'm a total beginner and I'm sorry if the question looks dumb. Suppose we have 2 parts hitting each other: For example a falling cube impinging a grounded plate. I need to transfer the impact forces on the grounded plate from the Dynamic Designer Motion to the SE-FEM simulation. The only constraint I have is a 3D contact between the two parts and when I want to add loads to SE simulation it opens an "Unassigned Load Entities" window saying that I need to select a load-bearing face/edge for my 3D contact constraint, but no matter how much I try I'm not able to select anything!

 

Any help would be very appreciated!

4 REPLIES 4

Re: Trouble with defining the load-bearing face for a 3D contact constraint in DDM-SE

Gears Phenom Gears Phenom
Gears Phenom

If you have not already contacted DDM support directly, I highly suggest doing so.

 

I used DDM in my past life and can tell you from personal experiance that those guys are top notch.

 

ddm.support@design-simulation.com

 

 

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Re: Trouble with defining the load-bearing face for a 3D contact constraint in DDM-SE

Experimenter
Experimenter
Thanks for the reply! Ok, I'll do that then Smiley Happy

Re: Trouble with defining the load-bearing face for a 3D contact constraint in DDM-SE

Gears Phenom Gears Phenom
Gears Phenom

IF you talk to Scott Z. tell him I say hello! 

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Re: Trouble with defining the load-bearing face for a 3D contact constraint in DDM-SE

Experimenter
Experimenter
Sure Smiley Happy Thank you Matt Smiley Happy