Cancel
Showing results for 
Search instead for 
Did you mean: 

Trying to create a muliple BOM for variable assys

Experimenter
Experimenter

BOM - Variable.gif

I can create a bill of materials for an as drawn and opposite handed part, where each BOM is laid above each other. But what I would like is for there to be muliple BOMs Eg. -01 is as drawn, -02 is the opp hand od -01 and a additionally add -03 variable of -01 and on ... Is this possible ?

Could it be generated from an excel spred sheet but still be linked to the models to regenerate any changes

4 REPLIES 4

Re: Trying to create a muliple BOM for variable assys

Hi,

 

Maybe need this for you!?

 

http://solutions.unitec.de/f/35154-70422/

http://www.all4edge.de/downloads/

 

Open an ASM model and after open xls from all4edge and run macro in the xls.

 

Tibor

Re: Trying to create a muliple BOM for variable assys

Gears Phenom Gears Phenom
Gears Phenom

I've been trying to create matrix BOMs since version 9.  Still can't do it with ST9.


____________________________________
--Scott Wertel, P.E.

Re: Trying to create a muliple BOM for variable assys

Hi,

 

You can made BOM list in 3d.

 

(view in My Videos)

 

Tibor

Re: Trying to create a muliple BOM for variable assys

Honored Contributor
Honored Contributor

My solution would be to insert a model vew into draft for each parts list. Then create a parts list for each one.

 

That gets the draft where you want it, does not matter how you get there.

 

I don't use family of parts or assemblies because long ago I found that they don't work with my assembly driven sheet metal models for some reason (At least that was the case in ST6/ST7)