Cancel
Showing results for 
Search instead for 
Did you mean: 

Tutorial not working

N/A

The next button on the Tutorial dialog does not display. I'm assuming this is a
problem cause by IE7.
See that attached DOC file.
1 REPLY

Re: Tutorial not working

N/A
Mitchel,
This is an intermittent problem during setup. From time to time customers
report this symptom.
What's happening is that hhactivex.dll does not get properly registered. I
don't know all the ins and outs of Setup, but setup shecks to see if you
have the file and if not, setup installs and registers it. Setup failed to
register it properly.
When customers report this problem, they have fixed it running "regsvr32
c:\windows\system32\hhactivex.dll" from a command line.
Click on Start
Click on Run
Copy and pase the following in the combo box.
regsvr32 c:\windows\system32\hhactivex.dll
Click on OK.
It should work properly now.
Regards,
Rick B.