Cancel
Showing results for 
Search instead for 
Did you mean: 

Two Separate Assemblies

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

I have two assemblies into one. To create added memory, I would like to separate the two and put then in two different files. I tried to highlight each part no go. Any thoughts!

 

Thank You

Greg

3 REPLIES 3

Re: Two Separate Assemblies

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Greg,

 

Not sure this is going to yeild the result you're hoping for....you already have the two assemblies [commonly refered to as "sub-assemblies"]....and assuming they're different.

 

The actual assembly file doesn't take up much space on a PC, as the component [par, psm] files themselves are where the physical size is carried.....assembly is just a "configuration" [a viewport, if you will] of those files.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Two Separate Assemblies

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

You might consider using the Transfer command.

 

It will allow you to move specific parts and sub-assemblies to a new (original) assembly structure.

Re: Two Separate Assemblies

Phenom
Phenom

Greg, I would work on simplifying or remodeling the geometry/elements you have if you're having RAM issues even with the very high end BOXX setup you're working with. From what I've seen, your models have a lot of splinter elements and unnecessary geometry that is repeated dozens to hundreds of times and really bogs down the software.

-Dylan Gondyke