Cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to get property 'empty' of undefined or null reference

Experimenter
Experimenter

i am getting the following error when trying to navigate in the file open dialog or  when trying to open a file after searching. this is in sharepoint btw.

Any idea what may be causing this issue?

Has been working fine and all of the sudden i start to get this error.

 

error.jpg

4 REPLIES

Re: Unable to get property 'empty' of undefined or null reference

Gears Phenom Gears Phenom
Gears Phenom

i would suggest getting in touch with your VAR and/or GTAC... 

 

If you have not heard.. Insight and Sharepoint for SE are both going to EOL over the next 2 releases...

 

not saying this is directly your issues...  but if 1 leads to the other, thought you should know.

 


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Unable to get property 'empty' of undefined or null reference

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

We're running Insight and it seems like I've occasionally and randomly seen this error. If I recall I just hit the "no" button and am good to go. It's rare though.

Is it constant and repeatable or unpredictable?

Internet Explorer, our SharePoint interface, occasionally "stops working" too.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Unable to get property 'empty' of undefined or null reference

Experimenter
Experimenter

it is constant on only the one PC.

 

every other pc works as it should.

Re: Unable to get property 'empty' of undefined or null reference

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you're on maintenance call GTAC as @Johnson_BigMatt suggests.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200