Cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to install fast search st9

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi guys, 

 

I'm having a problem while installing fast search ST9. The installation cant be done since there is existing solid edge st9 installed. 

 

Things i have tried but still cant work:

 

1. Remove all solid edge with its components and delete the registry by using SECleanUpAll. I reinstall the solid edge ST9 followed by fast search ST9 but the same problem occur.

2. Installing fast search first and it work. However I still cant install solid edge ST9 and the problem become vice versa. 

 

Hope you guys can help. Thanks in advance

9 REPLIES

Re: Unable to install fast search st9

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

There is a Fast Search installer for the server. Is that what you are installing?

If your files are local then you don't need to install that.

LMGi
www.TLMGi.com

Re: Unable to install fast search st9

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hi,

 

it is not possible to install the fast search on the client machine.

 

You can only install the fast search on an server where no Solid Edge is installed and your data is stored.

 

If you are the only user of Solid Edge, there is no need to install the fast search.

 

Hope this helps you.

 

Re: Unable to install fast search st9

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Okay noted on that. Btw can you help me with this? As in the picture there is a fast property search in the options, but in my solid edge there is no such thing. Thats the reason why i'm trying to install fast search in the first place. Is there any way so that i can access this function?

Untitled.jpg

Re: Unable to install fast search st9

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Okay noted on that. Btw can you help me with this? As in the picture there is a fast property search in the options, but in my solid edge there is no such thing. Thats the reason why i'm trying to install fast search in the first place. Is there any way so that i can access this function?

Untitled.jpg

Highlighted

Re: Unable to install fast search st9

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Strange, i looked in the comparison chart,i found no limititation regarding Fast search....

 

All the other things are there?

 

Datamanagement Tab, File Management Tab in the Options?

 

What License are you using?

 

Or wait, did you only install Solid Edge or also Insight or SEEC Client??

 

Check this maybe that is the reason.

 

Hope you will get this fixed, because i installed only Solid Edge and it was there....

 

Regards

 

Christian

Re: Unable to install fast search st9

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

I dont have  Datamanagement Tab, File Management Tab in the Options,

 

And i also Installed solid edge along with insight. Is this the main reason for the problem?

Re: Unable to install fast search st9

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Yes i think this is the Problem.

 

You can not use Insight and the Built in Datamanagement Functions togehter.

 

Insight or Built in Datamanagement.

 

You have to decide what is your favorite Datamanagement Solution for Solid Edge.

 

 

 

 

Re: Unable to install fast search st9

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I agree.

You have to uninstall the Insight client AND use a license without the Insight feature.

At least that was how it was with the initial release. I have not tried it since MP1.

LMGi
www.TLMGi.com

Re: Unable to install fast search st9

Solution Partner Genius Solution Partner Genius
Solution Partner Genius
I have MP1, still the same as in the initial Release