Cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to move an imported STL construction face

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Edgers,



I just have recognized, that with ST10 MP5 I'm not longer able to move/rotate a Surface_Mesh_Body using the steering wheel.

 

This was possible when we started with ST10, but I can't say when or with which MP it got impossible.

 

If the imported STL file builds a closed volume and it is handled as Design_Mesh_Body, then everything works fine.

 

 

PS.: You can move/rotate the steering wheel, and You see the changing values, but the geometry still keeps its position. Moving the mouse over that geometry afterwards, seems to show the edges of moved geometry, but shaded image still is a sbefore.

 

Strange behaviour.

Does anybody else see it too?

 

 

regards
Wolfgang
5 REPLIES

Re: Unable to move an imported STL construction face

Gears Phenom Gears Phenom
Gears Phenom

Hi @hawcad,

 

I've tested it and works well on my PC.

 

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Unable to move an imported STL construction face

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @Imics

 

 

thanks for info, one question: Which operating system?

 

 

regards
Wolfgang

Re: Unable to move an imported STL construction face

Gears Phenom Gears Phenom
Gears Phenom

Hi @hawcad,

 

Here is my specification:

 

Summary report (03/21/2018):

 Solid Edge 2019 64-bit information:
   FileVersion: 219.00.00.69
   ProductVersion: 219.00.00.069 x64
   Elapsed session time: 0:00:00:02
   Internal session time: 0:00:00:01
   Cumulative session time: 0:00:33:01
 System information:
   Sold-to ID:
   Owner:
   Company:
   User: SzucsI
   Computer: SZUCSIHPW, HP, HP ZBook 17 G4, x64-based PC
   Operating System: Microsoft Windows 10 Pro Version 1703 64 bites (Hungarian) 10.0.15063
 Processor information:
   Intel(R) Core(TM) i7-7700HQ CPU @ 2.80GHz, GenuineIntel
   Physical:1, Core:4, Logical:8, HT:Enabled, Clock:0.3Ghz
 Global memory status (inuse/avail/total):
   Physical: 6628MB/9634MB/16263MB, PageFile: 8668MB/10027MB/18695MB, Virtual: 226MB/134217501MB/134217727MB, Load: 40%
   Process: 187,80MiB (committed), 38,87MiB (reserved), 131071,78GiB (free)
   GDI objects: 167, USER objects: 6
 Video adapter information:
   Adapter: Intel Corporation, Intel(R) HD Graphics 630, 21.20.16.4590, Hybrid
   ChipSet: Intel(R) HD Graphics Family, Internal, 86MB
   Bios Info: Intel Video BIOS
   GDI Driver: CDD.DLL (21.20.16.4590)
   ICD Driver: C:\Windows\System32\DriverStore\FileRepository\igdlh64.inf_amd64_8c587880ddec6926\ig9icd64.dll.DLL (21.20.16.4590)
   Topology: Heterogeneous(Adapter,DPI,Model,Vendor),DPIAware
   Display: [1,2,1,0]Generic,1920x1080@60Hz,{v=128x128,p=128x128}dpi,100%,Intel(R) HD Graphics 630,Internal,Primary; [2,1,4,2]B24-8 TS Pro,1920x1080@60Hz,{v=92x92,p=92x92}dpi,100%,NVIDIA Quadro P4000,DP_EXT
 Application information:
   AppDisplay(Ac,Hx);RegionMode(Unset);Stereo(No);3DI(No);Effects(DC,MA,TF,MF);Scale(100%);
   Culling(Yes,20%);DynTransition(Yes,50%);AutoSharp(Off);Shaded(RP,HS);Glow(0);GAA(None);GFR(100%);

 

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Unable to move an imported STL construction face

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Imics

 

 

thanks for giving that info.

But I had to stop reading immedeately after seeing "Solid Edge 2019" !!!

 

 

So You are lucky to have the opportunity of being a beta tester.

 

I think it is not good to compare a 2019 with a ST10

Assume that there will be differences/changes which can lead to a different result too.

 

 

regards
Wolfgang

Re: Unable to move an imported STL construction face

Gears Phenom Gears Phenom
Gears Phenom
Hi,

Sorry this was my mistake. The stl moving test was running in ST10 MP5, it worked well as I mentioned. The sysinfo.exe was running from SE2019 to show software environment...

BR,
Imics
http://solidedgest.wordpress.com/