Cancel
Showing results for 
Search instead for 
Did you mean: 

Underlining Text Profile in part

Dear all,

 

There are some options availeble in the Text Profile promt screen, however I am missing the underlining option.

Reason for this is that I have to create a text with underlining according the DNV rules and I am not able to do so.

-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10
3 REPLIES

Re: Underlining Text Profile in part

I did a work around, created the text and draw a rectangle below it.
But still would find it better to have this in 1 feature.
-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10

Re: Underlining Text Profile in part

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Good workaround @DanielMCMLXXXII

  

Another option would be to download an underlined font from sites like http://www.1001fonts.com/underlined-fonts.html

 

Not sure if this would comply with company drafting standards, so you may have to search a closely resembling underlined font.

 

2016_Sep_12_01.png

Re: Underlining Text Profile in part

That is also an option.
Just got a mail from our dealer:


IR Description: Text underlining in Text Profile function

 

Dear Customer,

Your recent call to the Global Technical Access Center, Incident Report (IR)
Number 7805065 opened on 12-SEP-2016, has been researched by our GTAC
software engineers. They have determined that this perceived problem is
an enhancement to the current software functionality.

This IR was converted into an enhancement request (ER) on 12-SEP-2016
and is now referenced as ER Number 5765629. It is not currently scheduled
for implementation.

-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10