Cancel
Showing results for 
Search instead for 
Did you mean: 

Unexpected SE issue

Gears Phenom Gears Phenom
Gears Phenom

Hi All,

 

I faced today an unexpected SE issue. Cannot open the ASY file because of that :

 

se issue.png

 

Any suggestions how to get access to the ASY file ?

 

I have to admit that I am able to open subassemblies with no problem.

 

Thank you,

 

Arek

12 REPLIES 12

Betreff: Unexpected SE issue

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @arekkul

 

there could be several reason for that message.

 

  • as mentioned do You have permission to read that file
    is the network (suppose the file on a server) available
  • were any problems the last time the file was used?
    Was there a network problem when savin it the last time?
  • Has anybody else used that file and - for example -saved it with an academic license?

 

What You can try is to rename the corresponding .cfg file and try to open it then again

 

I remember there were situations where the problem was only in the config file rather than in the assembly file itself.

 

Give it a try!

 

regards
Wolfgang

Betreff: Unexpected SE issue

Gears Phenom Gears Phenom
Gears Phenom

Hi Wolfgang,

 

thank you for reply,

 

I have done your way, but no success. I have deleted the .cfg file as well, no success.

 

So I started to rebuild my ASY from the beginning.

 

Regards,

Arek

Betreff: Unexpected SE issue

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @arekkul

 

 

and are there no backupts from yesterday on which You can refer to?

 

regards
Wolfgang

Betreff: Unexpected SE issue

Gears Phenom Gears Phenom
Gears Phenom
Yes, I have backup, but with the same error.

Thank you,

Regards,

Arek

Betreff: Unexpected SE issue

Legend
Legend

Do you work from on a network?

 

Because your file can become corrupt when you save and at same time something happens with your network.

 

We have had the same problem a couple of times, Siemens can repair it (Not always) but will take around 1-2 weeks.

Sander
The Netherlands

Re: Unexpected SE issue

Siemens Genius Siemens Genius
Siemens Genius

try to open with another user account.  I had similar issue with .dft file and something has been corrupted at user's profile (registry entries)

Re: Unexpected SE issue

Gears Phenom Gears Phenom
Gears Phenom
Hi Tomas,


Yes, you have right. I tried to open it on 2 different machines,

no results,


Regards,


Arek

Betreff: Unexpected SE issue

Gears Phenom Gears Phenom
Gears Phenom

depending on the nature of corruption...  and the complexity of the assembly...  it might be worth submitting to GTAC for review and recovery.

 

but,  depending on the amount of work it would take to rebuild...  


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Unexpected SE issue

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @arekkul

 

 

 

there is one another approach You can try.

 

Open a new assembly and try to put the old one into that.

 

If this is possible YOu can move the parts up to the new top assembly and save it again.

So You will get a repared ASM with all Your parts in it and with all relations as before

This sometimes works better than open it.

 

regards
Wolfgang