Cancel
Showing results for 
Search instead for 
Did you mean: 

Unreadible .dft file

Experimenter
Experimenter

Hi, I have a file made by SE 2D st8, that is not possible to be opened nor from old version, neither with new ST9 installed in the new PC.

 

I recovered an older version dated 29 sept, and it is not readible, too. I am quite sure to have opened it in middle of september, no problem.

Older backup could be avaiable, but I believe to loose part of recent modifications.

File is a very large one since it was the repository of several schemes stored along the time (33MB).

Any hint to recover at least part of the job? Other files do not show that problem.

 

Thanks for any help

8 REPLIES 8

Re: Unreadible .dft file

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Davide_NTC, What message are you getting?

 

What type of license was your ST8 software?  If it was a University/Student license and you are now attempting to use a different license like the commercial or Free2D license, you may not be able to open the file due to the restriction imposed on the educational licenses where the files saved in those licenses connot be opened in the other license types.

 

Of course in the very odd chance that the file has become corrupt and you are under a maintenance agreement, you can have it submitted to development for inspection and possibly a fix.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Unreadible .dft file

Experimenter
Experimenter

Hi, thanks for fast reply.

Previous version was free/2D as the newer one.

File was unreadible with both ( casually it happened just before a programmed change of my PC, so I had the possibility to try open it with two different PCs,  and two different versions).

 

No service agreement, we use it for a marginal documentation task, but the affected file was a container of many schemes. Any idea?

 

 

 

Re: Unreadible .dft file

Experimenter
Experimenter

 

Meaning is : Impossible to open file: Be sure that file is of right format and version, and to have write access permissions.

error ST9.png

Re: Unreadible .dft file

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

@Davide_NTC wrote:

 

Meaning is : Impossible to open file: Be sure that file is of right format and version

 


Right there, it's talking about wrong versions, so what Ken has described especialy at the end that the file needs to be reported to GTAC to fix unless it is opened with the correct version of SE.

Re: Unreadible .dft file

Experimenter
Experimenter

Hi,

I compared three .dft files: 1.dft and 2.dft that are ok, and 3.dft that is corrupted (33MB)

davide@zen:~/Scrivania/dft$ ls -al *
-rwxr----- 1 davide davide   604160 ott 20 21:29 1.dft
-rwxr----- 1 davide davide   526848 ott 20 21:29 2.dft
-rwxr----- 1 davide davide 34965504 ott 20 21:29 3.dft

 

a check with Linux file utility showed that it is not a permssions problem:

davide@zen:~/Scrivania/dft$ file *
1.dft: Composite Document File V2 Document, Little Endian, Os: Windows, Version 6.1, Code page: 1200, Locale ID: 1040, Author: davsan, Template: metric draft.dft, Last Saved By: davsan, Revision Number: 91, Last Printed: Fri Feb 10 15:02:12 2017, Create Time/Date: Mon Feb 27 10:55:20 2012, Last Saved Time/Date: Fri May  5 12:21:35 2017, Number of Pages: 0, Number of Words: 0, Number of Characters: 0, Name of Creating Application: Solid Edge, Security: 0
2.dft: Composite Document File V2 Document, Little Endian, Os: Windows, Version 10.0, Code page: 1200, Locale ID: 1040, Author: davsan, Template: iso draft.dft, Last Saved By: davsan, Revision Number: 108, Last Printed: Tue Dec 13 09:45:51 2016, Create Time/Date: Fri Oct 20 14:42:16 2017, Last Saved Time/Date: Fri Oct 20 14:43:44 2017, Number of Pages: 0, Number of Words: 0, Number of Characters: 0, Name of Creating Application: Solid Edge, Security: 0
3.dft: Composite Document File V2 Document, No summary info

 

A binary edit on 3.dft shows that a corruped section in file header is present, compared with the oter two files (if should be all FFh), maybe SE is not able to manage a file larger than 32MB?

 

00000000   D0 CF 11 E0 A1 B1 1A E1 00 00 00 00 00 00 00 00   ................
00000010   00 00 00 00 00 00 00 00 3E 00 03 00 FE FF 09 00   ........>.......
00000020   06 00 00 00 00 00 00 00 00 00 00 00 39 02 00 00   ............9...
00000030   10 00 00 00 00 00 00 00 00 10 00 00 83 02 00 00   ................
00000040   02 00 00 00 00 00 00 00 04 00 00 00 08 00 00 00   ................
00000050   81 00 00 00 01 01 00 00 81 01 00 00 01 02 00 00   ................
00000060   12 00 00 00 4A 02 00 00 4F 02 00 00 50 02 00 00   ....J...O...P...
00000070   51 02 00 00 52 02 00 00 53 02 00 00 54 02 00 00   Q...R...S...T...
00000080   55 02 00 00 56 02 00 00 57 02 00 00 58 02 00 00   U...V...W...X...
00000090   59 02 00 00 5A 02 00 00 5B 02 00 00 5C 02 00 00   Y...Z...[...\...
000000A0   5D 02 00 00 5E 02 00 00 1E 00 00 00 37 02 00 00   ]...^.......7...
000000B0   38 02 00 00 39 02 00 00 3A 02 00 00 3B 02 00 00   8...9...:...;...
000000C0   3C 02 00 00 30 00 00 00 31 00 00 00 32 00 00 00   <...0...1...2...
000000D0   33 00 00 00 34 00 00 00 35 00 00 00 36 00 00 00   3...4...5...6...
000000E0   37 00 00 00 38 00 00 00 39 00 00 00 3A 00 00 00   7...8...9...:...
000000F0   3B 00 00 00 3C 00 00 00 3D 00 00 00 3E 00 00 00   ;...<...=...>...
00000100   3F 00 00 00 41 00 00 00 43 00 00 00 44 00 00 00   ?...A...C...D...
00000110   45 00 00 00 46 00 00 00 47 00 00 00 48 00 00 00   E...F...G...H...
00000120   49 00 00 00 4A 00 00 00 4B 00 00 00 4C 00 00 00   I...J...K...L...
00000130   4D 00 00 00 4E 00 00 00 4F 00 00 00 82 00 00 00   M...N...O.......
00000140   50 00 00 00 51 00 00 00 52 00 00 00 53 00 00 00   P...Q...R...S...

 

 

Thanks for any help

Davide

Re: Unreadible .dft file

Siemens Phenom Siemens Phenom
Siemens Phenom

Honestly, you are making and spending more time  on this then necessary.  Solid Edge can handle files much, much larger than 32 MB.  Your file, for whatever unknown reason, has simply become corrupt.  If you have active software maintenance you can submit the file for potential repair.  Otherwise, you will need to restore the file from one of your backups.

 

 

Re: Unreadible .dft file

Experimenter
Experimenter

Thanks for reply,

indeed it was not a waste of time since I learned a lot of things in the meanwhile....

Restoring the files from an old backup, the file is now opened, I found that by unknown reasons, the entities named "connector" are no more editable: they appear on drawing but they are no more selectable in any way, editable or erasable.

Maybe I forgot some information on how to operate on them?

Thanks for any hint, regards

 

Re: Unreadible .dft file

Experimenter
Experimenter

SOLVED: Entities not selectable.. there is a setting on SELEC menu to include some entities or not. It was not selected by default on new release ST9

 

Nuova immagine bitmap.jpg