Cancel
Showing results for 
Search instead for 
Did you mean: 

Update Only Selected Drawing Views

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hello Edgers,

 

Solid Edge has the Update drawing view command in the context menu.

 

01.png

The attached macro contains the same functionality and :

1. Thus allows this command to be assigned to a button on the ribbon or the radial menu and hence also enables assigning a KB shortcut, to be pressed after selecting a view.

2. Additionally, allows multiple views to be selected which are all updated at once, instead of multiple right-clicking and updating one view at a time.

 

 

Another macro useful for updating views only on the active sheet posted earlier is here.

 

Tushar Suradkar

www.SurfAndCode.in

www.CADVertex.com

 

1 REPLY

Re: Update Only Selected Drawing Views

Gears Phenom Gears Phenom
Gears Phenom

My Friend,

 

Thank you for your macros! All is great and they will help customers!!!!

 

BR,

Imics
http://solidedgest.wordpress.com/