Cancel
Showing results for 
Search instead for 
Did you mean: 

Update Views on Selected Sheets

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hello Edgers:

 

Delighted to post the third of 'view updating' macros and also the combined utility.

The previous view updating macros are update only selected drawing view(s) and Update views only on current sheet.

 

The attached macro allows selecting drawing sheet(s) from a list and updates all views on those sheets.

 

01.png

 

The UI additionally has buttons for the previously shared macros, which can also be called directly from the ribbon as in image above.

 

A short video illustrating the usage:

 

 

~Tushar Suradkar

www.CADVertex.com

www.SurfAndCode.in

 

5 REPLIES 5

Re: Update Views on Selected Sheets

Gears Phenom Gears Phenom
Gears Phenom

My Friend,

 

I have no any words for this! Cool!

 

Thank you for all what you do for Solid Edge!!!

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Update Views on Selected Sheets

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Thanks Imi.

 

Regards,

~Tushar

www.SurfAndCode.in

 

Re: Update Views on Selected Sheets

Valued Contributor
Valued Contributor

This works very well. But it would be even better with one more feature. Would it be possible to add a checkbox, which if checked would perform Ctrl+Shift Update Views? Doing this seems to have better results.

Re: Update Views on Selected Sheets

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Thanks for the feedback @kjm

I don't know what the Crtl+Shift Update View does; never heard of this.

Once I understand, will try to include the feature you suggest.

Re: Update Views on Selected Sheets

Hi Tushar,

 

Yes, thanks all macros (Sheet names table,Revision notes) and Solid Edge Video Quick Tip videos on youtube.

 

Tibor