Cancel
Showing results for 
Search instead for 
Did you mean: 

Update everything button?

Honored Contributor
Honored Contributor

Has anybody made a macro to update everything within a drawing?

 

Here are the things I'm aware all need to be touched to really update

Update active level

Update all open documents

Update all relationships

inspect/update physical properties

 

When that does not really update everything, then I also go open up the assembly, NOT through the draft. I believe there are model issues checked when opening the assmbly directly that are not checked when opened through draft. I say this because if my model has a problem, it opens about 10 times faster through the draft vs. opening it on it's own.

 

All rolled into a single button=update everything

 

Save all would not be a bad addition to this.

4 REPLIES

Re: Update everything button?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I'm surprised you've gotten no replies. The last place I worked had an add-in that when you hit save it would go through an update of all items you mentioned. It made saving painfully slow on large files so sometimes and we ended up turning it off.

As for your speed opening from the draft I was thinking it's because your cache would have the model files loaded when you open the draft. But you aren't in a managed environment, right? So you'd have no cache.

Anyway, I can inqure for the name of the add-in from the old colleagues.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Update everything button?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @12GAGE,

 

I'm sure that @Tushar would have [or create] something at a reasonable fee.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Update everything button?

Honored Contributor
Honored Contributor

I was thinking Tushar could show up in this thread.

 

I'm not in a managed environment. However I do use a very organized sheet metal tank part numbering system.

 

I don't really want the update tied to saving. The typical issue is getting the changes to carry through so I can see the result to make the next decision.

Re: Update everything button?

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

That's right. The letter r is now gone out of the word free Smiley Happy