Cancel
Showing results for 
Search instead for 
Did you mean: 

Update view macro

Valued Contributor
Valued Contributor

Has anyone come across a macro to open drafts, update views and save again, to a list of draft files?

Nathan M. Gardner

https://www.etsy.com/people/NathanMGardner

Be sure to check out my work!!
Made in Maine Wood Carvings

5 REPLIES

Re: Update view macro

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

You have it too.

 

Look for this:

c:\Program Files\Solid Edge ST6\Custom\OpenSave\

open_save.jpg

 

BR,

 

Imics
http://solidedgest.wordpress.com/
Highlighted

Re: Update view macro

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

give one that prints also

Re: Update view macro

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Have you tried the Print Drawings command under the Application button?  When you are prompted to open a file, you use CTRL and SHIFT to select multiple DFT files to batch print.

 

In the same Custom folder , there is also a Batch macro that can batch print using folders and it can also batch translate as well.



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com

Re: Update view macro

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

already use batch. i want something that will print, stop at a file to be updated, update the file continue printing

Re: Update view macro

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
I see. Well, the source code for Batch and OpenSave is delivered with the programs and VB .net Express is free, so you could modify one or the other to do what you want.


Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com