Cancel
Showing results for 
Search instead for 
Did you mean: 

Usability of etch in SE

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Hi All,

 

Is it just me or is etch completely unusable? We are looking to make a label from two layer plastic which requires the surface to be engraved. We have had good results with SE export using etch, so I thought a bigger label would be easy. However it bogs down so so so very very very badly with text it is basically unusable? Am I doing something wrong or are we just not meant to have any more than a couple of etched lines?

 

Shane

ST8 MP5

Shane Murray
SE2019 MP3
6 REPLIES 6

Re: Usability of etch in SE

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @shanefarra,

 

Not seeing any issues here......etching with either drawn or imported graphics & text, or even a combination.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Usability of etch in SE

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

I'm going to try SP6. Also having a lot of issues with sketches disappearing as well. Not really sure what is going on, but I don't want to spend half a day reconfiguring everything to clear my profile...

Shane Murray
SE2019 MP3

Re: Usability of etch in SE

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

What kind of a PC are you running?  Sounds maybe graphics card related...



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Usability of etch in SE

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Operating System
Windows 7 Professional 64-bit SP1
CPU
Intel Core i7 4790K @ 4.00GHz 27 °C
Haswell 22nm Technology
RAM
16.0GB Dual-Channel DDR3 @ 799MHz (11-11-11-28)
Motherboard
Gigabyte Technology Co., Ltd. Z97-HD3 (SOCKET 0) 28 °C
Graphics
241PLY (1920x1080@60Hz)
2260W (1920x1080@60Hz)
Intel HD Graphics 4600 (Gigabyte)
4095MB NVIDIA Quadro K2200 (NVIDIA) 31 °C
Storage
111GB Samsung SSD 850 EVO 120G SCSI Disk Device (SSD) 26 °C
931GB Western Digital WDC WD10EZEX-00BN5A0 SCSI Disk Device (SATA) 25 °C
Optical Drives
ASUS DRW-24D3ST SCSI CdRom Device
Audio
Realtek High Definition Audio

Shane Murray
SE2019 MP3

Re: Usability of etch in SE

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Hi,

 

After some careful investigation, it would appear that it is the font that I have used to create it that causes the time delay. As for the disappearing sketches, I have absolutely no idea

Shane Murray
SE2019 MP3

Re: Usability of etch in SE

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

All I can suggest for the disappearing sketches is maybe check your NVIDIA driver...  Not sure what else it might be.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com