Cancel
Showing results for 
Search instead for 
Did you mean: 

User defined table in drafting

Experimenter
Experimenter

How we can merge two cells of two adjacent column?

 

Thanks

sachin

4 REPLIES 4

Re: User defined table in drafting

Genius
Genius

Hey,

 

You can only merge cels in one colum if them values are the same.

SE ST9 + TC 10.1.7

Re: User defined table in drafting

Experimenter
Experimenter

Thanks for your reply...

It dont allow to merge cells if they are in one column also.

What I observed is that, if I create rows under the "Header" and not as "Data" cells, it allows me to merge in one column and with different column also.

Re: User defined table in drafting

Genius
Genius

I only use FOP Table and BOM in SE, in other case I use Excel tables.

SE ST9 + TC 10.1.7

Re: User defined table in drafting

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I believe you can only merge Column Headers horizontally.  The cell data can only be merged vertically.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com